SSZTBK7 march 2016
In my first, gripping installment of this series, I explained qualitatively how charge pumps work – while skillfully leaving out any numbers. But numbers are what it’s all about in the end, and you can’t design anything properly until you know what components to use. In this installment, I’ll explain the effect that external components have on performance.
Figure 1 shows an unregulated charge pump that operates with a duty cycle of 0.5 and whose output voltage is nominally twice the input voltage. In practice, the output voltage of the charge pump is less than 2VI and is given by Equation 1:
where IO is the output current and RO is the output resistance.
Figure 1 Unregulated charge
pumpAs long as the flying capacitor is big enough, the output resistance, RO, depends only on the rDS(on) of transistors Q1 through Q4. If you do the math (frankly, I don’t recommend it), you end up with Equation 2 for the output resistance:
where f is the switching frequency; C is the flying capacitance; and R is the resistance of the charge and discharge paths, assuming they are all equal. (If Q1 and Q2 are the same and Q3 and Q4 are the same, then R = rDS(on)(Q1) + rDS(on)(Q4).)
which is math talk for saying that it looks almost like two
straight lines, as shown in Figure 2.
The curve in Figure 2 is the key to understanding charge-pump operation. What it tells
you is that if C is larger than some critical value, it has almost no effect on the
output impedance. This critical value occurs when
. Actually, the output impedance is 1.3 times the minimum value
when
, but in the same way that
straight-line approximations are a useful simplification in Bode plots, it’s easier
just to make sure that your flying capacitor is bigger than
.
Figure 2 Output impedance of Figure 1A few more mathematical gymnastics show that for large values of flying capacitance, the peak current in the charge pump during steady-state operation is equal to twice the output current. During startup, when the flying capacitor charges up from 0 V to ≈VI, the peak current can be significantly higher. Well-designed charge pumps gradually increase the gate-source voltage of the FET switches during startup, which acts as a soft-start and limits the peak current.
Equation 3 calculates the output voltage ripple:
CO is the output capacitance.
Don’t forget that ceramic capacitors exhibit a DC-bias effect, which means that the effective capacitance in a circuit is often a lot less than the nominal value. Double-check the effective capacitance at VI for the flying capacitance and VO for the output capacitor.
In a regulated charge pump, an adjustable current source (or sink for an inverting charge pump) typically controls the output voltage, as shown in Figure 3.
Figure 3 Equivalent circuit of a fully
integrated regulated charge pumpSince this circuit only has three
switches, the output impedance tends to
when C is very large. However, since the current source,
IDRV, needs a certain minimum voltage across it, VDROP, in
order to operate correctly, the maximum output voltage of the circuit in Figure 3 (assuming C is larger than the critical value) is given by Equation 4:
As long as the output voltage is less than this maximum value, the regulation loop of the charge pump will reduce the output impedance to such a small value that it has almost no effect on the output voltage in practice.
Note that the results are slightly different (although still the same shape) if the charge pump uses diodes for any of the switches or if the duty cycle is not 0.5. I’ll cover those results in the next installment.