SSZTCT2 april   2015 CC1120 , CC1125 , CC1190

 

  1.   1
  2.   2
    1.     3
    2.     Ease of Installation
    3.     Communication Robustness
    4.     Long Battery Life

Terje Lassen

What problems could you solve if you had a connected smart city sensor that could live for over 10 years without maintenance? Innovation in RF connectivity now enables many new ways for cities to manage resources, making them greener, more efficient and more convenient. Myriads of sensors are finding their way into the everyday life of a city, managing energy consumption, routing traffic, monitoring air quality, improving waste management, monitoring and controlling street lighting, etc. Most of these sensors only have tiny amounts of data to send, hence the existing cellular system, optimized for high bandwidth, streaming smartphones, is often not a good fit. For smart city applications, a long range, ultra-narrow band network addresses the three key challenges for successful deployment of an autonomous sensor network: Ease of installation, communication robustness and long battery lifetime.

Ease of Installation

The installer is a person that typically has had very limited knowledge and training on the actual system and node functionality. First pass installation success must be very close to 100% to allow for a cost-effective deployment.

Communication Robustness

Maintaining information flow from a major deployment of sensor nodes require high communication success rate. Scrambling an RF savvy person to debug in-field communication issues is very expensive. For long term stability of the network, it is critical to use a robust communication link that also has the capacity and co-existence performance to support the projected growth of the connected devices. The network must run without issues both today and in 10 years from now!

Long Battery Life

Changing a battery is a very expensive operation. Therefore, the battery needs to last for the lifetime of the product. Although for some applications, energy harvesting can be an option, today this is typically a far more expensive solution than using a battery with sufficient capacity for the lifetime of the product.

The biggest smart city application today is smart metering. If you take for instance a gas meter, a typical requirement is between 10-20 years of battery lifetime. The cost of no communication is to send a person out to read the meter, so communication reliability is critical for the profitability of the installation. A large part of these meters today use narrowband and UNB (ultra-narrowband) communication to assure communication reliability, scalability and range to cover a whole city. UNB is the best choice to get robust, long range communication, and can achieve the best range in a real world environment. Check out this video where you can see TI demonstrating UNB achieving more than 100 km RF communication range using CC1120 and CC1190.

More than 100 km range with no data loss using long range narrowband

There is a push in the market to move to standards based solutions. Narrowband is defined in the key IEEE 802.15.4g spec, and narrowband is also selected for all new gas meter deployments in e.g. France and Italy (wM-Bus N-mode). Narrowband is the only technology that can offer the required network scalability, robust long-range communication and interoperability across multiple silicon providers. See also the white paper: Long-Range RF Communication: Why Narrowband is the de Facto Standard for more information on narrowband vs. other long-range communication technologies.

There is a definite trend for smart cities to move beyond only smart meter applications. The possibility to deploy low-cost sensor nodes with high communication reliability and years of battery lifetime opens for new application areas. Some examples of these applications are:

Street lighting: Remote monitoring and control of lighting reduces power consumption and make maintenance more efficient, which in turn gives more reliable streetlights for the communities.

GUID-CA6A920B-EDCC-41D9-9B40-CAEEDDED367D-low.jpg

Parking sensors: Route traffic to available parking spots gives city planners better insight into actual usage for better planning of future parking lots. In a city, automatic tracking of available parking spots can typically increase the usage of a parking spot. For spots with parking meters, the cost of a connected parking sensor can therefore often be justified, as it gives a positive return for the owner of the parking meter.  The success of a smart city application usually depends on the return of investment calculation, to move beyond small scale trials and prototypes, someone needs to save substantial cost or increase revenue to justify the expense – with ease of use, robustness and longer battery life solutions from TI, we are pushing down the barrier for innovative smart city applications.

Air quality sensors: In many countries regulations mandate maximum levels for gases and pollution in cities. To assure compliance, sensors need to be placed around the city. Using narrowband technology with e.g. CC1120 in a dedicated sensor network will typically be a much more cost effective solution compared to e.g. using cellular connection. Please note that CC1125 has a slight better narrow band performance than CC1120 or CC1125, meaning you can reach longer distances.

In summary, for the smart city, using ultra-narrow band technology for long range communication will enable a robust, cost-effective network with longer battery lifetime. Narrowband is the best choice to assure capacity and reliability for innovative applications also in the years to come, with a projected dramatic increase of connected devices.

To read more posts related to connected living, check out these resources: