SWRA774 may 2023 IWRL6432
Figure 2-1 A
Representative Radar Based Classification
ChainFigure 2-1 depicts the typical processing flow of an algorithmic chain that incorporates an ML-based classifier. First basic physical layer processing is done on the raw ADC data received from the radar front end. This block involves a series of FFTs to separate the signal based on range, Doppler, and angle of arrival [2]. In some cases (e.g. Case-Study-1: Motion Classification), this can additionally be followed by detection and tracking algorithms.
The next step involves feature extraction, where the output of the previous block is processed to provide input to an ML-based classifier. The choice of feature extraction and the corresponding classifier that follows are closely coupled. Some popular options found in the literature [3] are listed below:
There is a tradeoff between the intelligence in the feature extraction block and the complexity of the classifier. Approach (3) typically results in the lighter-weight classifier. The selection of the feature extraction block and the classifier architecture depends on the complexity of the classification task as well as requirements such as classifier performance, frame rate, and available memory and computing power.
In a typical implementation on the IWRL6432, the radar physical layer (PHY) processing is handled by the HWA while the classifier runs on the MCU (M4F). Hand-crafted feature extraction typically runs on the M4F with some assistance from the HWA.