SWRZ138 july 2023 AWRL1432
ADVANCE INFORMATION
Continuous Wave Streaming CZ mode: Sudden jump in RX output codes every 20.97152 msec
AWRL1432ES1.1
On Continuous Wave Streaming CZ mode, the Rx data shows a sudden jump in output codes every 20.97152 milliseconds.
This is not an issue in the Radar Functional mode when chirps are used. However, this issue will be seen when testing Rx chain in lab using continuous stream mode.
In order to use Continuous stream (CW) mode for testing, it is recommended to start data capturing from the first sample itself to make sure the glitch occurs at deterministic samples. Please follow the below sequence to achieve this:
The glitch will not be seen with this sequence. For example, if the user analyzes first 20ms of data or between 21 and 41ms.