Internal Bus access to SPI for data transfer not supported when SPI smart-idle mode is enabled.
Revision(s) Affected
IWRL1432ES1.1,
ES2.0
Details
Smart-idle mode needs to be disabled for SPI before the first trigger for data transfer access. If the SPI smart-idle mode is required to be enabled, it has to be enabled again once the access is complete.
Workaround
It is recommended to follow the below sequence:
Auto Wake-up = 1 & Controller mode
- Configure McSPI as required
- Enable SmartIdle (by setting LPRADAR:APP_CTRL:SPI1_SMART_IDLE_ENABLE for SPI1 and LPRADAR:APP_CTRL:SPI2_SMART_IDLE_ENABLE for SPI 2 )after ensuring that there is no pending transaction from/to SPI or any more access to be done to McSPI by CPU or DMA
- If any register or memory access to McSPI has to be done, disable SmartIDLE mode (by setting LPRADAR:APP_CTRL:SPI1_SMART_IDLE_ENABLE=0 for SPI 1 and LPRADAR:APP_CTRL:SPI2_SMART_IDLE_ENABLE =0 for SPI 2)
- In Controller mode, the external host is not going to toggle the SPI_CS, hence there will not be any wakeup => there is no difference between (LPRADAR:APP_CTRL:SPI1_SMART_IDLE_AUTO_EN is 1 or 0 for SPI 1 and LPRADAR:APP_CTRL:SPI2_SMART_IDLE_AUTO_EN is 1 or 0 )
Auto Wake-up = 1 & Peripheral mode
Configure McSPI as required
- Enable SmartIdle (by setting LPRADAR:APP_CTRL:SPI1_SMART_IDLE_ENABLE for SPI1 and LPRADAR:APP_CTRL:SPI2_SMART_IDLE_ENABLE for SPI 2 ) after ensuring that there is no pending transaction from/to SPI or any more access to be done to McSPI by CPU or DMA
- If any register or memory access to McSPI has to be done by any master (DMA / CPU), disable SmartIDLE mode (by setting LPRADAR:APP_CTRL:SPI1_SMART_IDLE_ENABLE=0 for SPI 1 and LPRADAR:APP_CTRL:SPI2_SMART_IDLE_ENABLE =0 for SPI 2)
- If there is wakeup from McSPI (because of some SPI_CS toggle), then the clock is automatically enabled.
- Disable SmartIdle configuration (by setting LPRADAR:APP_CTRL:SPI1_SMART_IDLE_ENABLE=0 for SPI 1 and LPRADAR:APP_CTRL:SPI2_SMART_IDLE_ENABLE =0 for SPI 2 ) to do the register access.
The below table shows the Register Addresses for above workaround.
| Bits |
Name |
Address |
| 0 |
LPRADAR:APP_CTRL:SPI1_SMART_IDLE_ENABLE |
0x560603A8 |
| 2 |
LPRADAR:APP_CTRL:SPI1_SMART_IDLE_AUTO_EN |
0x560603A8 |
| 0 |
LPRADAR:APP_CTRL:SPI2_SMART_IDLE_ENABLE |
0x560603AC |
| 2 |
LPRADAR:APP_CTRL:SPI2_SMART_IDLE_AUTO_EN |
0x560603AC |