TIDA039 January   2025

 

  1.   1
  2.   2
  3.   Trademarks

This application brief details the design considerations of the discrete power design for the AC8025 (from AutoChips™) system-on-chip (SoC) power rails with a power-management IC (PMIC) design. The design uses the TPS6593-Q1 PMIC, TPS62875-Q1 synchronous buck converters, and TPS745-Q1 low-dropout (LDO) regulators. The original power source is the battery. Then the battery voltage is converted to regulate the 5V or 3.8V bus. The LM25149-Q1 converts the battery voltage to regulate the bus voltage. All components in this design are automotive-qualified.

The TPS6593-Q1 IC has five buck converters and four LDOs. This PMIC is non-volatile memory (NVM) programmable, meaning the default register values are set in the TI production line to the desired values for this platform without further need for the customer to change settings. The full orderable part number for this one-time-programmable (OTP) spin is TPS6593C4C8RWERQ1. See the Technical Reference Manual for the specific part number for more details on the OTP settings.

This power design is an example of how required rails for AC8025 can be powered with TI PMIC, synchronous buck converters, and LDOs. This power design is possible to customize and optimize based on the actual use case regarding the SoC variant, current requirements, used peripherals, and so forth.

Design Parameters

Table 1 shows the power rails, load requirements, and power group.

Table 1 Power Rails, Load Requirements, and Power Group
Power RailVoltage (V)Current (A)Power Group
LPDDR4, LPDDX41.125
D1V1_DDR1.15
IVI_D1V81.83.53
IVI_A1V81.83
SFT_0V80.80.52
IVI_D3V33.33.54
IVI_A3V33.34
VDDQ_0V60.60.36
SFT_1V81.80.153
SFT_3V33.30.154
RTC_0V80.80.152
RTC_1V81.80.153
VCORE_0V80.8—1
IVI_A0V80.81
UFS_1V21.223
RTC_3V33.30.154

Power Design

Figure 1 shows a block diagram with LM25149-Q1, TPS6593-Q1, TPS62875-Q1, TPS628502-Q1, and TPS784-Q1 devices powering the AC8025 SoC power rails.

The main features of this power design include the following:

  • Power sequencing for AC8025 rails are controlled with PMIC TPS6593-Q1
  • The GPIO output on the TPS6593-Q1 device can be used to control the TPS62875-Q1, TPS628502-Q1, and TPS784-Q1 devices for power sequencing
PMP41107, TIPA-020001 AC8025 Power Tree Block
                    Diagram Figure 1 AC8025 Power Tree Block Diagram

Sequencing

Figure 2 shows an example power-up timing of the power rails and power group corresponding signals.

PMP41107, TIPA-020001 Power Sequencing Figure 2 Power Sequencing

Schematic

Figure 3 shows the LM25149-Q1 schematic with critical components. For layout guidance, see the corresponding device data sheet and EVM user guide.

PMP41107, TIPA-020001 LM25149-Q1 Schematic Figure 3 LM25149-Q1 Schematic

Figure 4 shows the TPS6593-Q1 and the LDO TLV793P-Q1 for MCU power supply schematic with critical components. For layout guidance, see the corresponding device data sheet and EVM user guide. For LDO input and output capacitor values, see the data sheet recommendation.

PMP41107, TIPA-020001 TPS6593-Q1 and the LDO for MCU
                    Schematic Figure 4 TPS6593-Q1 and the LDO for MCU Schematic

Figure 5 shows the TPS62875-Q1 schematic with critical components. For layout guidance, see the corresponding device data sheet and EVM user guide.

PMP41107, TIPA-020001 TPS62875-Q1 Schematic Figure 5 TPS62875-Q1 Schematic

Figure 6 shows the TPS628502-Q1 schematic with critical components. For layout guidance, see the corresponding device data sheet and EVM user guide.

PMP41107, TIPA-020001 TPS628502-Q1 Schematic Figure 6 TPS628502-Q1 Schematic

Figure 7 shows the TPS784-Q1 schematic with critical components. For layout guidance, see the corresponding device data sheet and EVM user guide.

PMP41107, TIPA-020001 TPS784-Q1 Schematic Figure 7 TPS784-Q1 Schematic

Summary

The design outlined in this application brief, using the LM25149-Q1, TPS6593-Q1, TPS62875-Q1, TPS628502-Q1, and TPS784-Q1 provides the power requirements for AutoChips AC8025 SoC while maintaining good efficiency. This design is compact due to the minimum number of external components. The I2C control allows for diagnostic testing and other control of the TPS6593-Q1 device.