TIDT321 January 2023
Output voltage ripple is shown in the following figures.
The waveform in Figure 3-3 was created using the following conditions: input voltage = 565 VDC; output
power = full load.
Figure 3-3 Output Voltage Ripple (23
VOUT)The waveform in Figure 3-4 was created using the following conditions: input voltage = 565 VDC; output
power = full load.
Figure 3-4 Output Voltage Ripple (5
VOUT)