TIDT324 February 2023
#FIG_Z3J_FHK_2MB to #FIG_CVJ_JNM_JWB show the output voltage start-up waveforms at 12-V input and –8-V output with the converter starting up into no load and into 2.7-A constant-current load using the electronic load. Two methods of enabling the converter were exercised and captured: one where the input voltage is already turned ON and the converter waits for the enable signal to go HIGH; the other where the enable signal is tied to VIN and the converter waits for the main power supply to be turned ON.
Figure 3-8 Start-Up Into No Load, 12-V
Input, –8-V Output, Start-Up Initiated via the Enable Connection (input Supply
Already Turned ON)
Figure 3-9 Start-Up Into 2.7-A
Constant-Current Load, 12-V Input, –8-V Output Start-Up Initiated via the Enable
Connection (input Supply Already Turned ON)
Figure 3-10 Start-Up Into No Load, 12-V Input, –8-V Output, Start-Up Initiated via Input
Supply (Enable Signal Already Set HIGH)
Figure 3-11 Start-Up Into 2.7-A Constant-Current Load, 12-V Input, –8-V Output, Start-Up
Initiated via Input Supply (Enable Signal Already Set HIGH)