TIDT345 September 2023
Load transient response waveforms are shown in the following figures. The first response is from 0.75 A to 2.25 A and the next response is from 2.25 A to 0.75 A
Figure 3-17 Load Transient at 48-V Input,
Figure 3-19 Load Transient at 48-V Input,
Figure 3-18 Load Transient at 48-V
Input,
Figure 3-20 Load Transient at 48-V Input,