TIDT380 February 2024
Start-up behaviors of the LM5152-Q1 are shown in the following figures.
Figure 3-2 Start-up at 4.2
VIN, 8.5 VOUT, 11.76A IOUT
Figure 3-3 Start-up at 13.5
VIN, 13.5 VOUT, 7.48A IOUT
Figure 3-4 Start-up at 18 VIN,
18 VOUT, 5.55A IOUTStart-up behaviors of LM74900-Q1 are shown in the following figures.
Figure 3-5 Start-up at 18 VIN, 18 VOUT, 5.78A IOUT
Figure 3-6 Start-up at 4.2 VIN, 4.2 VOUT, 24A IOUTStart-up behaviors of LMQ644A2-Q1 are shown in the following figures.
Figure 3-7 Start-up at 8.5 VIN, 6 VOUT, 6A IOUT
Figure 3-8 Start-up at 13.5 VIN, 6 VOUT, 6A IOUT
Figure 3-9 Start-up at 18 VIN, 6 VOUT, 6A IOUT
Figure 3-10 Start-up at 8.5 VIN, 3.3 VOUT, 3A IOUT
Figure 3-11 Start-up at 13.5 VIN, 3.3 VOUT, 3A IOUT
Figure 3-12 Start-up at 18 VIN, 3.3 VOUT, 3A IOUTStart-up behaviors of TPS7B81-Q1 are shown in the following figures.
Figure 3-13 Start-up at 4.2 VIN, 6 VOUT, 0.15A IOUT
Figure 3-14 Start-up at 13.5 VIN, 6 VOUT, 0.15A IOUT
Figure 3-15 Start-up at 18 VIN, 6 VOUT, 0.15A IOUTStart-up behaviors of TPS745-Q1 are shown in the following figures.
Figure 3-16 Start-up at 3.3 VIN, 1.8 VOUT, 0.5A IOUTStart-up behaviors of the TPS628503-Q1 are shown in the following figures.
Figure 3-17 Start-up at 3.3 VIN, 1.8 VOUT, 3A IOUT