TIDUEI1C November 2018 – April 2020
The TIDEP-01010 provides a reference for creating a area scanner or safety guard application using TI’s IWR6843, based on 60-GHz mmWave radio-frequency complementary metal-oxide semiconductor (RF-CMOS) technology. Frequency-modulated continuous-wave (FMCW) radars enable accurate measurement of distances and relative velocities. Thus, radars are useful for detection of occupancy and whether an object or person has entered a space of interest.
In area scanner or light curtain safety-guard applications, where it is important to have precisely defined "keep-out" zones, the ability of radar to accurately localize detected objects can be used to implement multiple detection zones and trigger corresponding responses. A single radar deployed to equipment with a critical "keep-out" perimeter could implement a multi-stage response, so that when an object or person first approaches the perimeter, a moderate warning flag is raised. Then, if the perimeter is breached, a critical response is triggered.
With the widespread growth of factory automation, there is a greater need for smarter incident management solutions that can detect the movement of people and objects around heavy machinery while maintaining productivity. Using TI's 60-GHz mmWave sensors, both presence detection and the ability to gauge the object's trajectory and speed are enabled. Thus, a system can be created that can dynamically adjust the safety zone's size depending on the object's speed of approach, alert before a safety zone is breached while also ignoring objects whose trajectory is not towards the zone.
An important advantage of radars over camera and light-detection-and-ranging (LIDAR)-based systems is that radars are relatively immune to challenging environmental conditions common in industrial facilities such as dust and smoke. Because FMCW radars transmit a specific signal (called a chirp) and process the reflections, they can work in both complete darkness and bright daylight (radars are not affected by glare). When compared with ultrasound, radars typically have a much longer range and faster transit time for their signals.
The IWR6843AOP variant features a short-range, wide field of view antenna-on-package (AOP), achieving unprecedented levels of integration in an extremely small form factor.
The AoP sensor design addresses three main challenges for robotics or factory automation: