TIDUEY3 November 2020
The mmWave software development kit (SDK) enables the development of mmWave sensor applications using the AWR6843AOP SOC and EVM. The SDK provides foundational components that allow end users to focus on their applications. In addition, the SDK provides several demonstration applications, which serve as a guide for integrating the SDK into end-user mmWave applications. This reference design is a separate package installed in addition to the SDK package, and is the application portions of the block diagram.
Figure 2-2 mmWave SDK Software Block Diagram