A GUI developed with Python is included with this
reference design. Figure 3-8 shows a screen capture of the GUI. In addition to the graphical view, the data
that is displayed is also presented live in a terminal window as shown in Figure 3-9.
To use the smoke detector GUI:
- The smoke detector GUI is distributed via Python
source code, and must be built into an executable before use. Unzip the file
containing the Python source code, and refer to the accompanying
README for instructions on building the GUI. - Connect the SASI sensing board to the LaunchPad
Development Kit. Only the integrated XDS110 emulator on the LaunchPad is needed
for PC communication. The rest of the LaunchPad is not activated.
- Connect the LaunchPad to the PC via USB
cable.
- Open the GUI
sasi_smoke_detector_m0l1306.exe.
- Make sure to start with
clean air.
- Wait for 12 seconds after
first time power up or reset for proper calculation of base
signal.
- Click the Update COM button for COM port
auto-detection.
- Enter the filename for data logging.
- The log file is stored in
the
capture\<date>\folder along with an image of
the GUI plot.
- Multiple logs are
appended with “_0”, “_1”, and so forth.
- Each file logs 1000
entries, and a new file is generated every 1000 entries.
- Set the smoke trigger threshold value in the
Least Significant Bit (LSB).
- Click the Start button to start
measurement.
- Measurement statistics
are displayed on the side in LSB.
- Smoke indication (no
smoke or smoke detected) is also displayed based on whether the signal
exceeds the threshold.
- Estimated particle size
and mass concentration are also displayed.
- Click the Stop button to stop
measurement.
- Data is automatically
logged. Time and signal response in LSB from the IR and Blue LEDs,
particle size estimation, and the smoke detection flag are also streamed
to the terminal.