TIDUF70 April 2024
The test signal is a wideband OFDM (Orthogoanl Frequency Divistion Multiplexed) modulated signal operating at a 5GSPS data rate. The patterns are configured with a 2GHz and 4GHz signal bandwidth. Figure 3-2 and Figure 3-3 show the spectrum performance out of the transmitter.
The modulated output signal is looped back to the transmitter through a 20dB attenuator to maintain that the receiver is not over-driven. Figure 3-4 and Figure 3-5 show the FFT spectrum of the captured waveform from the receiver.