VIDEO SERIES
C2000™ enhanced pulse width modulator (ePWM)
The enhanced pulse width modulator on C2000 devices controls many of the power-related systems found in many end equipment. The ePWM peripheral module is responsible for generating pulse signals that are fed into controls systems as well as other parts of the device, such as the ADC SOC. The ePWM module consists of 8 submodules which each serve a distinct function within the ePWM. The submodules are: time-base, counter compare, action qualifier, dead-band, PWM chopper, event trigger, trip-zone, and digital compare.
C2000™ enhanced pulse width modulator (ePWM)
C2000™ Enhanced Pulse Width Modulator (ePWM): Overview
This is the first video in the C2000 ePWM video series, which covers type 4 ePWMs.
00:03:27|22 Apr 2022
This is the first video in the C2000 ePWM video series, which covers type 4 ePWMs. This video provides a general overview of the ePWM perihperal by briefly describing the submodules within the peripheral and overviewing the methods to configure the ePWM module.