VIDEO SERIES
C2000™ SysConfig
C2000™ SysConfig
C2000™ SysConfig: Overview
This is the first video in the C2000™ SysConfig video series. In less than 5 minutes, learn about the most important benefits of the SysConfig tool
This is the first video in the C2000™ SysConfig video series. In less than 5 minutes, learn about the three most important benefits of the SysConfig tool and how it greatly simplifies the C2000™ development process.
SysConfig provides intuitive and facilitated code generation through its user interface. Users can configure the initialization settings for their C2000 device through an assortment of input boxes and drop-down selections, and the SysConfig tool will automatically generate the relevant DriverLib code needed for device configuration.
SysConfig also includes PinMux functionality built-in, which allows it to automatically assign pins to device modules. Furthermore, SysConfig creates portable code which allows for simplified device-to-device transition. SysConfig is available in a wide variety of platforms for users.