How do I add, edit or delete a payment method for a myTI company account?

If you are in an administrator or buyer role:

  1. Log in to your myTI company account dashboard.
  2. Under Ordering, select Payment methods.
  3. On the Payment methods page:
    1. To add a payment method, click the Add New button in the upper right-hand corner.
    2. To edit a payment method, click the Pencil icon. (Note that editing a payment method used in one or more checkout profiles will affect each of those profiles.)
    3. To delete a payment method, click the Delete icon.
  4. Once you are done with your edits, return to the Payment methods page to confirm your changes.

Please note that it is only possible to edit or delete Apruve accounts at this time.