Using JTAG with the UCD3138: Exporting the contents of a CCS file via JTAG
00:01:49
|
2016 년 03 월 14 일
This video demonstrates how to export the contents of flash to a file after programming. Please note that this can be a time consuming operation, so it is recommend doing this as a once off verification step only. Checksum based verification is a much more time efficient way of ensuring that the flash is programming correctly in a production setting.
리소스
이 비디오는 시리즈의 일부입니다.
-
디지털 전원 컨트롤러 소개
video-playlist (42 videos)