Inventory

Inventory

When a future inventory date is showing on TI.com for a device, what does it mean?

The future inventory date shows an estimation of when TI expects to have more inventory available for a given device. These estimated timeframes are subject to change at any given time.

When showing future inventory dates for devices, what does "week of" mean?

When you see a future inventory date showing for a device, "week of" means that the device could stock up anywhere during the entire week (Sunday to Sunday) from the date that is given. For example, if the future inventory date says "More unites week of 19 Dec 2021", this means we expect to have more inventory available anywhere from December 19 to December 26.

When do I see future inventory dates for some devices and not others?

This is intentional an you will only see future inventory dates for a subset of devices on TI.com.