DSP Applications Journal Web PageGray Rule
  
1Q 2001 Edition

The DSP Applications Journal is designed to highlight practical engineering solutions using TMS320 DSPs in typical applications. Where applicable, users will find software routines and program structures.

Contents

Note: To view the following links, Acrobat Reader 4.x is required.

Hardware/Board Design

Emulation Fundamentals for TI's DSP Solutions (SPRA439A)
Explanation of the setup of the emulator hardware systems for single and multiprocessor applications as well as how the system components interact during debug. A troubleshooting guide will be provided to assist in commonly found setup problems.
File size: 698 kbytes

TMS320C621x/C761x EDMA Queue Management Guidelines (SPRA720)
It is important to know what types of transfers are performed by the EDMA, how they are requested, and how multiple transfers interact while being serviced. This knowledge allows transfers to be programmed so they take full advantage of the EDMA and obtain the maximum bandwidth available from the device.
File size: 137 kbytes

How to Begin Development Today with the TMS320C6414 and the TMS320C6415 DSPs (SPRA718)
Existing C6000™ software tools and development platforms can be used to develop code for the C6414, C6415, and C6416 because they are compatible. This capability allows for systems to be up and running quickly. File size: 131 kbytes

TMS320C6000 BGA Manufacturing Considerations (SPRA429)
PCB design techniques that improve manufacturing quality and reliability. File size: 100 kbytes

TMS320VC5416 Bootloader (SPRA602)
Features and operation of the TMS320VC5416 Bootloader and the contents of the on-chip ROM. File size: 271 kbytes

Software Programming Techniques

A Case Study in DSP Systems Integration - The TI Third Party Vocoder Demonstration (SPRA734)
A case study approach that explains how TI Vocoder Technology Demonstration Kit allows users to graphically configure multiple channels of several speech-coding algorithms running on a TMS320C6000™ Digital Signal Processor (DSP). File size: 148 kbytes

How Are High-End DSPs Suited for the AES Algorithms (SPRA740)
An investigation of how well high-end DSPs are suited for 5 Advanced Encryption Standard (AES) algorithms and compares the optimized implementations of the algorithms on a state-of-the-art DSP. File size: 159 kbytes

TMS320C6000™ DSP Multiprocessing with a Crossbar Switch (SPRA725)
A focus on the data-passing technique provided by a bi-directional first-in first-out (BiFIFO) interface to a crossbar switch. The TMS320C6000 DSP is used here to illustrate the requirements and implementation for a wireless base station application. File size: 140 kbytes

Development Software and Tools

Real-Time Analysis in an eXpressDSP Algorithm (SPRA732)
Methods of embedding DSP/BIOS APIs in the algorithm and implementing the Real-time Trace Control Interface (IRTC) interface. It also describes how the IRTC interface is used in a typical DSP application. File size: 167 kbytes