How do I add, edit or delete an address for a myTI company account?

Only those in an administrator or buyer role can add, edit or delete addresses. To do so:

  1. Log in to your myTI company account dashboard.
  2. Under Ordering, select Addresses.
  3. On the Addresses page:
    1. To add an address, click the Add new button in the upper right-hand corner.
    2. To edit an existing address, click the Pencil icon. (Note that editing an address used in one or more checkout profiles will affect each of those profiles.)
    3. To delete an address, click the Delete icon.
  4. Once you are done with your edits, return to the Addresses page to confirm your changes.

Find answers to your ordering questions

Explore other ways to find answers