Seleccione una versión
MSP432WARE
MSP432Ware for MSP432™ Microcontrollers
Standalone MSP432Ware 3.50.00.02 for Windows
Standalone MSP432Ware 3.50.00.02 for Linux
Standalone MSP432Ware 3.50.00.02 for Mac OS X
MSP432Ware Pack for Keil
Documentación
Recomended CCS Download
BSD Release of MSP432 Driver Library
MSP432Ware Release Notes
Información de la versión
Click on the links in the table below to download.
MSP432Ware is a collection of code examples, datasheets and other design resources for ALL MSP432 devices delivered in a convenient package - essentially everything developers need to become MSP experts!
Novedades
- Updating documentation regarding MSP432 RevB vs MSP432 RevC
- Added MSP Flasher command line programmer
- Added MSP432 Security and Update Tool
Install/Upgrade
There are two methods to install MSP432Ware:
Installing via the Code Composer Studio (CCS) App Center
If you have CCS 6.0 or later you can install MSP432Ware via the CCS App Center.
Installing via the Standalone Installer
If CCS is not your primary IDE or want an offline installer on hand you can download the standalone installer.
FAQ
What is the difference between MSP432Ware and Driver Library?MSP432Ware is a collection of MSP430 and MSP432 software and tools. One of the main components of MSP432Ware is Driver Library (DriverLib).
Why are there multiple driverlib folders within MSP432Ware?MSP432Ware contains many different software libraries and projects. Some of these components depend on a specific version of Driver Library. Each component ships the version of Driver Library they tested with to ensure that all software works for you out of the box.
Can I have multiple versions of MSP432Ware installed?Yes! MSP432Ware installations can exist alongside each other. You should only see the latest installed version within the TI Resource Explorer window of Code Composer Studio however.
How can I get support for MSP432Ware?Feel free to use the TI E2E forum to ask anything MSP432Ware related.