4 Revision History
Changes from Revision D (December 2018) to Revision E (January 2021)
- Added Functional Safety bulletGo
Changes from Revision C (August 2018) to Revision D (December 2018)
- Changed front page to remove second descriptionGo
- Deleted Gate-Drive Current figure Go
- Added SL2 pin to the continous shunt amplifier input pin voltageGo
- Added SL2 pin to the continous shunt amplifier input pin voltageGo
- Changed IN1 to IN1/PH and IN2 to IN2/EN Go
- Changed MODE typical pulldown resistance Go
- Added MODE typical pullup resistanceGo
- Changed Wording in VDS Configuration section Go
Changes from Revision B (March 2017) to Revision C (August 2018)
- Changed the Features and Descriptions sectionsGo
- Changed the type of the SL2 pin from O to I in the Pin Functions tableGo
- Changed SPI parameter name conventionsGo
- Changed the VDS(OCP) from 0.86 V to 0.96 V in the OCP
Threshold Voltage graphGo
- Changed the I(CHOP) equation in the Current Regulation and Current Chopping Configuration sectionsGo
- Changed the current equation in the Amplifier Output (SO) sectionGo
- Changed the description of the WD_EN bit in the IDRIVE and WD Field Descriptions tableGo
Changes from Revision A (November 2016) to Revision B (March 2017)
- Changed
the maximum voltage for AVDD from 5.7 to 5.75 in the Absolute Maximum Ratings tableGo
- Changed maximum VSP value for GAIN_CS = 00 and GAIN_CS = 10 for the DRV8703-Q1 amplifier gain parameter in the Electrical Characteristics tableGo
- Added the R(VDRAIN) note to the External
Components tableGo
- Changed one resistor value from 32 kΩ to 65 kΩ in the MODE Pin Block Diagram
Go
- Changed what happens when a fault condition is no longer present in the Overcurrent Protection (OCP) sectionGo
- Deleted AV × from tthe I(CHOP) equation in the Current Chopping Configuration sectionGo
Changes from Revision * (October 2016) to Revision A (November 2016)
- Released the full version of the data sheet Go