SNVS532D October 2007 – August 2020 LM5067
PRODUCTION DATA
If the LM5067-2 is in use, after the Fault Timeout Period described above, CT is discharged by the 2.5 µA current sink to 1.25 V. The TIMER pin then cycles through seven additional charge/discharge cycles between 1.25 V and 4 V as shown in Figure 8-5. The restart time ends when the TIMER pin voltage reaches 0.3 V during the final high-to-low ramp. The restart time, after the Fault Timeout Period, is equal to:
For example, if CT = 0.33 µF, tRESTART = 3.1 seconds. At the end of the restart time, Q1 is switched on. If the fault is still present, the fault timeout and restart sequence repeats. The on-time duty cycle of Q1 is approximately 0.5% in this mode.