SBOS165B September 2000 – April 2024 OPA627 , OPA637
PRODMIX
Refer to the PDF data sheet for device specific package drawings
The electromagnetic interference (EMI) rejection ratio, or EMIRR, describes the EMI immunity of operational amplifiers. An adverse effect that is common to many operational amplifiers is a change in the offset voltage as a result of RF signal rectification. An operational amplifier that is more efficient at rejecting this change in offset as a result of EMI has a higher EMIRR and is quantified by a decibel value. Measuring EMIRR can be performed in many ways, but this report provides the EMIRR IN+, which specifically describes the EMIRR performance when the RF signal is applied to the noninverting input pin of the operational amplifier. In general, only the noninverting input is tested for EMIRR for the following three reasons:
A more formal discussion of the EMIRR IN+ definition and test method is provided in the EMI Rejection Ratio of Operational Amplifiers application note, available for download at www.ti.com.
The EMIRR IN+ of the OPA627 is plotted versus frequency (see Figure 6-8). If available, any dual and quad op amp device versions have nearly similar EMIRR IN+ performance. The OPA627 (SOIC package) unity-gain bandwidth is 45MHz. EMIRR performance below this frequency denotes interfering signals that fall within the operational amplifier bandwidth.
Table 6-1 shows the EMIRR IN+ values for the OPA627 (SOIC package) at particular frequencies commonly encountered in real-world applications. Applications listed in Table 6-1 can be centered on or operated near the particular frequency shown. This information can be of special interest to designers working with these types of applications, or working in other fields likely to encounter RF interference from broad sources, such as the industrial, scientific, and medical (ISM) radio band.
FREQUENCY | APPLICATION OR ALLOCATION | EMIRR IN+ |
---|---|---|
400MHz | Mobile radio, mobile satellite and space operation, weather, radar, UHF | 39dB |
900MHz | GSM, radio communication/navigation/GPS (to 1.6GHz), ISM, aeronautical mobile, UHF | 40dB |
1.8GHz | GSM, mobile personal communication, broadband, satellite, L-band | 50dB |
2.4GHz | 802.11b/g/n, Bluetooth™, mobile comm, ISM, amateur radio and satellite, S-band | 70dB |
3.6GHz | Radiolocation, aero communication and navigation, satellite, mobile, S-band | 85dB |
5GHz | 802.11a/n, aero comm and nav, mobile comm, space and satellite operation, C-band | 85dB |