SLVSA30D April 2011 – March 2019 UCD9090
PRODUCTION DATA.
Pins 22 and 23 can be used as GPIs or PWM outputs. These PWM outputs have an output frequency of 0.93 Hz to 7.8125 MHz.
The frequency for PWM1 and PWM2 is derived by dividing down a 15.625-MHz clock. To determine the actual frequency to which these PWMs can be set, must divide 15.625 MHz by any integer between 2 and (224-1). The duty cycle resolution will be dependent on the set frequency for PWM1 and PWM2.
The PWM1 or PWM2 duty cycle resolution is dependent on the frequency set for the given PWM. Once the frequency is known the duty cycle resolution can be calculated as Equation 2
To determine the closest frequency to 1MHz that PWM1 can be set to calculate as the following:
All frequencies below 238 Hz will have a duty cycle resolution of 0.0015%.