JAJSJG5 July 2020 ADS9226
PRODUCTION DATA
On the CS rising edge, both converters start converting the sampled value on the analog input, and the internal capacitors are switched to the REFP_x pins. Most of the switching charge required during the conversion process is provided by the external decoupling capacitor CREFP_x. If the charge lost from CREFP_x is not replenished before the next CS rising edge, the subsequent conversion occurs with this different reference voltage and causes a proportional error in the output code. To eliminate these errors, the internal reference buffers of the device maintains the voltage on the REFP_x pins.
All performance characteristics of the device are specified with the internal reference buffer and a specified value of CREFP_x. As shown in Figure 7-4, place a decoupling capacitor CREFP_x between the REFP_x pins and the REFM_x pin as close to the device as possible.