JAJSED0G May 2012 – January 2018 CDCM6208
PRODUCTION DATA.
The Smart Input MUX supports auto-switching and manual-switching using control pin (and through register). The Smart Input MUX is designed such that glitches created during switching in both auto and manual modes are suppressed at the MUX output.
SI_MODE1
PIN NO. 47 |
REGISTER 4 BIT 13 SMUX_MODE_SEL | REGISTER 4 BIT 12 SMUX_REF_SEL | REF_SEL
PIN NO. 6 |
SELECTED INPUT | |
---|---|---|---|---|---|
0 (SPI/I2C mode) | 0 | X | X | Auto Select Priority is given to Primary Reference input. | |
1 | 0 | 1 | Primary input | input select through SPI/I2C | |
1 | Secondary input | ||||
1 | 0 | Primary input | input select through external pin | ||
1 | Secondary input | ||||
1 (pin mode) | not available | 0 | Primary or Auto (see Table 6) | ||
1 | Secondary or Auto (see Table 6) |
Example 1: An application desired to auto-select the clock reference in SPI/I2C mode. During production testing however, the system needs to force the device to use the primary followed by the secondary input. The settings would be as follows:
Example 2: The application wants to select the clock input manually without programming SPI/I2C. In this case, program R4[13:12] = 11, and select primary or secondary input by toggling REF_SEL low or high.
SmartMux input frequency limitation: In the automatic mode, the frequencies of both inputs to the smart mux (PRI_REF divided by R and SEC_REF) need to be similar; however, they can vary by up to 20%.
Switching behavior: The input clocks can have any phase. When switching happens between one input clock to the other, the phase of the output clock slowly transitions to the phase of the newly selected input clock. There will be no-phase jump at the output. The phase transition time to the new reference clock signal depends on the PLL loop filter bandwidth. Auto-switch assigns higher priority to PRI_REF and lower priority to SEC_REF. The timing diagram of an auto-switch at the input MUX is shown in Figure 37.