JAJSC32E September 2012 – June 2019 DP83848-EP
PRODUCTION DATA.
This register contains the advertised abilities of this device as they will be transmitted to its link partner during Auto-Negotiation.
BIT | BIT NAME | DEFAULT | DESCRIPTION |
---|---|---|---|
15 | NP | 0, RW | Next Page Indication: |
0 = Next Page Transfer not desired | |||
1 = Next Page Transfer desired | |||
14 | RESERVED | 0, RO/P | RESERVED by IEEE: Writes ignored, Read as 0 |
13 | RF | 0, RW | Remote Fault: |
1 = Advertises that this device has detected a Remote Fault | |||
0 = No Remote Fault detected | |||
12 | RESERVED | 0, RW | RESERVED for Future IEEE use: Write as 0, Read as 0 |
11 | ASM_DIR | 0, RW | Asymmetric PAUSE Support for Full Duplex Links: |
The ASM_DIR bit indicates that asymmetric PAUSE is supported. | |||
Encoding and resolution of PAUSE bits is defined in IEEE 802.3 Annex 28B, Tables 28B-2 and 28B-3, respectively. Pause resolution status is reported in PHYCR[13:12]. | |||
1 = Advertise that the DTE (MAC) has implemented both the optional MAC control sublayer and the pause function as specified in clause 31 and annex 31B of 802.3u. | |||
0 = No MAC based full duplex flow control | |||
10 | PAUSE | 0, RW | PAUSE Support for Full Duplex Links: |
The PAUSE bit indicates that the device is capable of providing the symmetric PAUSE functions as defined in Annex 31B. | |||
Encoding and resolution of PAUSE bits is defined in IEEE 802.3 Annex 28B, Tables 28B-2 and 28B-3, respectively. Pause resolution status is reported in PHYCR[13:12]. | |||
1 = Advertise that the DTE (MAC) has implemented both the optional MAC control sublayer and the pause function as specified in clause 31 and annex 31B of 802.3u. | |||
0= No MAC based full duplex flow control | |||
9 | T4 | 0, RO/P | 100BASE-T4 Support: |
1 = 100BASE-T4 is supported by the local device | |||
0 = 100BASE-T4 not supported | |||
8 | TX_FD | Strap, RW | 100BASE-TX Full Duplex Support: |
1 = 100BASE-TX Full Duplex is supported by the local device | |||
0 = 100BASE-TX Full Duplex not supported | |||
7 | TX | Strap, RW | 100BASE-TX Support: |
1 = 100BASE-TX is supported by the local device | |||
0 = 100BASE-TX not supported | |||
6 | 10_FD | Strap, RW | 10BASE-T Full Duplex Support: |
1 = 10BASE-T Full Duplex is supported by the local device | |||
0 = 10BASE-T Full Duplex not supported | |||
5 | 10 | Strap, RW | 10BASE-T Support: |
1 = 10BASE-T is supported by the local device | |||
0 = 10BASE-T not supported | |||
4:0 | Selector | <00001>, RW | Protocol Selection Bits: |
These bits contain the binary encoded protocol selector supported by this port. <00001> indicates that this device supports IEEE 802.3u. |