JAJSOI8H November 2009 – May 2022 LMP8645 , LMP8645HV
PRODUCTION DATA
As seen in Figure 7-1, the current flowing through the shunt resistor ( RS) develops a voltage drop equal to VSENSE across RS. The resulting voltage at the –IN pin will now be less than +IN pin proportional to the VSENSE voltage.
The sense amplifier senses this indifference and increases the gate drive to the MOSFET to increase IS′ current flowing through the RIN+ string until the amplifer inputs are equal. In this way, the voltage drop across RIN+ now matches the votlage drop across VSENSE.
The RIN resistors are trimmed to a nominal value of 5 kΩ each. The current IS′ flows through RIN+ , the MOSFET, and RGAIN to ground. The IS′ current generates the voltage VG across RGAIN. The gain is created bythe ratio of RGAIN and RIN.
A current proportional to IS is generated according to the following relation:
where
This current flows entirely in the external gain resistor developing a voltage drop equal to:
This voltage is buffered and presented at the output with a very low output impedance allowing a very easy interface to other devices (ADC, μC…).
where