JAJSHO3D July 2019 – October 2022 SN3257-Q1
PRODUCTION DATA
Source leakage current is defined as the leakage current flowing into or out of the source pin when the switch is off. This current is denoted by the symbol IS (OFF).
Drain leakage current is defined as the leakage current flowing into or out of the drain pin when the switch is off. This current is denoted by the symbol ID (OFF).
The setup used to measure both off-leakage currents is shown in Figure 7-2.