JAJSHQ8D July 2019 – July 2021 TPS25832-Q1 , TPS25833-Q1
PRODUCTION DATA
The NTC input pin allows for user programmable thermal protection. See Electrical Characteristics for NTC pin thresholds. The NTC input pin threshold is ratiometric with VCC. The external resistor divider setting VNTC must be connected to the TPS25833-Q1 VCC pin to achieve accurate results. See Figure 10-28 and Figure 10-29. When VNTC = 0.5 × VCC (approximately 2.5 V typically), the TPS25833-Q1 performs two actions:
If the overtemprature condition persists causing VNTC = VCC × 0.65 (3.25-V typical), the TPS25833-Q1 turns off the buck regulator and pulls the LS_GD pin low. The THERM_WARN flag remains asserted; however, the FAULT pin is NOT asserted for this condition.
Tuning the VNTC threshold levels of VWARN_HIGH and VSD_HIGH is achieved by adding RSER, RPARA, or both RSER and RPARA in conjunction with RNTC. Figure 10-30 is an example illustrating how to set the THERM_WARN threshold between 75°C and 90°C with a ΔT between THERM_WARN assertion and device shutdown of 17°C to 28°C. Consult the chosen NTC manufacturer's specification for the value of β. It may take some iteration to establish the desired warning and shutdown thresholds.
Below is NTC spec and resistor value used in Figure 10-30 example.
The NTC resistor should be placed near the hottest point on the PCB. In most cases, this will be close to the SW node of the TPS25833-Q1, near the buck inductor, RSNS sense resistor and external MOSFETs (if used).