JAJSMF3A May 2022 – September 2022 TPS25985
PRODUCTION DATA
TPS25985x needs the SWEN pin to be pulled up to a supply rail which is powered up before the device is enabled. Failing this, the device is not able to turn on the output. The SWEN pullup supply must not be derived from the output of the eFuse. Use one of the following options to derive the pullup supply rail for SWEN.
Use an existing standby rail in the system, which is derived from the main power input and comes up before the eFuse is turned on.
Use an LDO (3.3 V or 5 V) powered from the main power input.
Use a Zener regular powered from the main power input.
Use the ITIMER pin of the primary eFuse. Ensure the ITIMER pin does not have excess loading which can interfere with the normal overcurrent blanking timer functionality.
The ground connections for the various components around the TPS25985 eFuses must be wired directly to each other and the GND pins of respective eFuses. This must be followed by connecting them to the system ground at one point. For more details, refer to TPS25985EVM eFuse Evaluation Board. Do not connect the various component grounds through the high current system ground line.