JAJSES0 February 2018 XTR305
PRODUCTION DATA.
The instrumentation amplifier has high-impedance NPN transistor inputs that do not load the output signal, which is especially important in current output mode. The output signal is a controlled current that is multiplexed either to the SET pin (to close the voltage output loop) or to IAOUT (for external access).
The principal circuit is shown in Figure 44. The two input buffer amplifiers reproduce the input difference voltage across RGAIN. The resulting current through this resistor is bidirectionally mirrored to the output. That mirroring results in the transfer function of Equation 6:
The accuracy and drift of RGAIN defines the accuracy of the voltage to current conversion. The high accuracy and stability of the current mirrors result from a cycling chopper technique.
The output current, IAOUT, of the instrumentation amplifier is limited to protect the internal circuitry. This current limit has two settings controlled by the state of M2 (see Electrical Characteristics: Instrumentation Amplifier (IA), Short-Circuit Current specification).
NOTE
If RSET is too small, the current output limitation of the instrumentation amplifier can disrupt the closed loop of the XTR305 in voltage output mode.
With M2 = low, the nominal RGAIN of 10 kΩ allows an input voltage of 20 VPP, which produces an output current of 4 mAPP. When using lower resistors for RGAIN that can allow higher currents, the IA output current limitation must be taken into account.