DLPU082C August 2021 – March 2024 DLPC7540
The first two steps in the GUI focuses on getting the prerequisite information from the user and the next two steps focuses on the Edge Blending.
The Manual Blending GUI page enables user to do both photometric corrections (brightness adjustments in the overlap region) as well as geometric corrections (angle adjustments of the keystone corners in the projected image).
Step 0 : Prerequisites
Before using the Manual Blending GUI page, please make sure that the following prerequisites are done.
When the connection is ready, use the Manual Blending page starting from Step 1 and go in the order of steps.
Step 1 : Read Parameters(A) Read Output Resolution
This is the first and foremost step in the process of Manual Blending to read the output resolution information from the projector system. The default value of Output Width is 0 and Output Height is 0. Clicking on the "Read Output Resolution" button populates the valid (>0) output resolution information if and only if the connection to the projector system has been established.
When the output resolution information has been read from the projector system, all other GUI elements that are relevant for the next step of action are enabled.
Note: Unless the output resolution information is populated, none of the following functionalities in the GUI would work as expected.
(B) Read Blending Data (Optional)
The user is given two options to either to read the manual blending parameter values stored in the EEPROM and populate into the fields in the page using the button "Load Blending Parameters and Geometric Correction Values from EEPROM" or manually enter data in the GUI in Step 2. When the blending parameter values from the EEPROM are loaded in the GUI, then the user can apply the same on the screen by clicking on the "Initialize and Apply" button in Step 2.
Step 2 : Initialization of Blending Parameters
This step focuses on getting multiple system information from the user to initialize the parameters that are required for edge blending in the following steps. The user is supposed to enter the following information:
Projectors Layout
Layout in which the projectors are arranged, that is, horizontally stacked (columns) or vertically stacked (rows) to combine the projected image.
Based on the values provided by the user, the table of rows and columns depicting the projector layout in the sections "Current Projector in the Layout", "Black Luminance Values (Nits)" and "White Luminance Values (Nits)" is changed to give a visual prepresentation of the projectors layout.
Current Projector in the Layout
In the table of rows and columns depicting the projectors layout, identify the projector system that is currently being blended, that is, the projector system to which the current instance of control program is connected to.
Input Source
Select the input source used to display the pattern or image that should be used for calibration. This calibration patternor image must match the output resolution of the system identified in Step 1.
By default, "Splash Pattern" is the input source that displays a built-in default calibration pattern used for the Manual Blending process.
If "External Source" is the input source selected, then the user is expected to display a custom calibration pattern through External Video Input. The option to "Keep the display as is" makes it so no updates are made to the display. This is the most useful option for quickly tuning the RGB values for Simple 1D RGB mode.
Overlap Information
The user is allowed to give the overlap and fusion zone information in either exact number of pixels or lines or as a percentage in both horizontal and vertical directions.
When the "Projectors Layout" has
The GUI controls are disabled when those values are not needed or used.
Photometric Correction Mode
For 2D cases and cases that include warping, "Use Black / White Luminance Values" must be selected. For 1D cases without warping, "Use Simple 1D RGB Gain / Offset Values" can be chosen.
Black Luminance Values (Nits)
White Luminance Values (Nits)
Simple 1D RGB Values
The RGB gain and offset values for the projector are entered in the below fields. The acceptable range of values are between 0 and 1 for all fields. TI recommends starting with the gain fields as all 1, and the offset fields as all 0. The gain values should be lowered so that a white field appears to be the same brightness as the least bright projector in the system. Raise the offset values to where the black field brightness of all projectors is the same.
After all of the above values are entered, click the "Initialize and Apply" button to initialize all the blending parameters and apply the values on the screen.
Step 3 : Geometric Correction
After the blending parameters are initialized, the user is allowed to perform the geometric correction only for the keystone corners.
Step 4: Enter Adjacent projector Geometric Parameters
For the 2D Luminance mode algorithm to correctly calculate the shapes of the overlapping regions, the keystone values of the adjacent projectors must be entered. The values can remain at default (unwarped) until all projectors in the system have completed the warping phase
Step 5:Apply Manual Blending Corrections to EEPROM