DLPU082C August 2021 – March 2024 DLPC7540
The controller has several pre-defined patterns that the user can select using TPG Pre-defined Pattern command. Use the DLP Control program tool to configure these pre-defined patterns the controller TPG block generates the pattern data. This option is useful for:
These are additional configuration commands specific to test patterns.
Command Name | Description |
---|---|
Set TPG Border | Set border around selected TPG, border width can be 0-20; and border color programmable (R,G,B) value in the range of 0-1023. |
Set TPG Resolution | Set the TPG pattern resolution. In case the resolution of the pattern is smaller than the display resolution of the DMD, controller will fill the area with pleasing color. |
Set TPG FrameRate | Configure TPG frame-rate between 30Hz-120Hz. There is dependency of the TPG resolution with regard to frame-rate; for example, in case of 4K resolution, the maximum frame-rate is limited to 60Hz, and in case of 1080p resolution, the maximum frame rate is limited to 240Hz. |