DLPU102B December 2020 – July 2022
The DLP LightCrafter Dual DLPC900 EVM is a flexible, ready-to-use evaluation module which, when coupled to one of the supported DLP LightCrafter Dual Controller DMD EVMs, enables the sending of customer created patterns from the DLPC900 Controllers to the attached DMD for display at the customer determined pattern rates. The DLP LightCrafter Dual DLPC900 EVM and supported DMD EVMs are offered for purchase separately so that customers can determine which elements they wish to piece together for their own application evaluation system.
The following items are not included with the EVM and need to be purchased separately if needed for customer evaluation: