DLPU102B December 2020 – July 2022
Upon execution of the DLP LightCrafter DLPC900 GUI application, the panel shown in Figure 4-1 is displayed. The GUI panel contains the following three sections:
In any of the GUI sections, clicking a Get button reads the current settings of that particular subsection. Clicking the Set button programs the settings into the respective subsection. Please note that some commands may require additional steps before the GUI display is updated.
If the text in the GUI does not display correctly please change the DPI settings. Right click on the executable and select Properties. On the Compatibility tab select the "Change high DPI settings" button. Change your settings as shown in High DPI Settings.