JAJSDQ6C June 2012 – September 2017
PRODUCTION DATA.
The device has an analog supply (AVDD). Drive these pins with a clean supply and connect bypass capacitors close to the pins. After power up, the device must be reset to set all internal registers to their default state. Resetting the device is done by applying an active low pulse on the RST pin after the power supplies stabilize. As part of the reset process, the AFE4300 sets all register bits to the respective default settings.
Some register bits must be written to values different from their default values after reset for proper operation. By default, the AFE4300 enters into a power-down state at start-up. The startup and initialization for the device is shown in Figure 16 and Table 6 lists the recommended timing values.
NOM | UNIT | ||
---|---|---|---|
t1 | Time between supplies turning on and an active RST | > 10 | ms |
t2 | Active RST duration | > 50 | µs |
t3 | Time between RST and register writes | > 1 | ms |