JAJSEB4F October 2017 – May 2022 TLIN2029-Q1
PRODUCTION DATA
The RXD output structure is an open-drain output stage. This allows the TLIN2029-Q1 to be used with 3.3- V and 5-V I/O processor. If the RXD pin of the processor does not have an integrated pull-up, an external pull-up resistor to the processor I/O supply voltage is required. The select external pull-up resistor value should be between 1 kΩ to 10 kΩ, depending on supply used (See IOL in electrical characteristics). The VSUP pin of the device should be decoupled with a 100-nF capacitor as close to the supply pin of the device as possible.