SBAA607A December 2023 – January 2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P4 , AMC1303M2520 , AMC1305L25 , AMC1306M25 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Figure 4-7 shows the clock signal SD1_C1 which is input to GPIO123 and the phase shifted data signal SD1_D1 which is input to GPIO122. In this test setup GPIO123 is inverted by the software, as shown below.
// Set 3-sample qualifier for GPIO122 and GPIO123 and do not invert GPIO123
GPIO_SetupPinOptions(123, GPIO_INPUT, GPIO_INVERT | GPIO_QUAL3);
GPIO_SetupPinMux(122,GPIO_MUX_CPU1,7); // MUX position 7 for SD1_D1
GPIO_SetupPinMux(123,GPIO_MUX_CPU1,7); // MUX position 7 for SD1_C1
The data SD1_D1 is now sampled by F28379D SDFM at the falling edge of SD1_C1, which corresponds to the rising edge of the inverted clock signal at GPIO123 input. The data sampled by the F28379D was always logic ‘0’, validated though output of the Sinc3 OSR64 filter = -16384 in Code Composer Studio, as shown below.
In conclusion the method of clock signal compensation by inverting the clock input of the GPIO input in software was validated. By inverting the clock, a fixed delay of half of the clock period is added to the clock signal which can be sufficient to meet the TMS320F28379D setup and hold of minimum timings of 10 ns for the SDFM qualified GPIO (3-sample) mode 0. However, each system design needs to be checked individually if the resulting timings for setup and hold of the MCU for the SDFM qualified GPIO (3-sample) mode 0 can be met.