SCDU038 April   2024 TMUX6221 , TMUX7221

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
  6. 2Hardware
    1. 2.1 Power Requirements
    2. 2.2 Setup
    3. 2.3 Jumper Information
    4. 2.4 Test Points
  7. 3Hardware Design Files
    1. 3.1 Schematics
    2. 3.2 PCB Layouts
    3. 3.3 Bill of Materials (BOM)
  8. 4Additional Information
    1. 4.1 Trademarks

Jumper Information

For the left side header, pin 1 is at the top left corner pin (denoted as an X). The right side header has pin 1 (denoted as an X), which is at the top right corner. Table 3-1 shows the jumper configurations. Note: U1 refers to the signal pathway that connects to the U1 10-pin DGS footprint.

Table 2-1 Generic Jumper Pinout Map
Jumper IDPin 1Pin 2Pin 3Pin 4Pin 5Pin 6

J1

Floating

VDD

GND

U1 Pin 1

GND

VSS

J2

FloatingVDDGND

U1 Pin 2

GNDVSS

J3

FloatingVDDGNDU1 Pin 3GNDVSS

J4

FloatingVDDGNDU1 Pin 4GNDVSS

J5

FloatingVDDGNDU1 Pin 5GNDVSS

J6

FloatingVDDGNDU1 Pin 6GNDVSS

J7

FloatingVDDGNDU1 Pin 7GNDVSS

J8

FloatingVDDGND

U1 Pin 8

GNDVSS

J9

FloatingVDDGND

U1 Pin 9

GNDVSS

J10

FloatingVDDGND

U1 Pin 10

GNDVSS

Check the device specific data sheet for the pin-out. For power (VDD or VSS) and ground (GND), lines connect shunts on the appropriate jumpers to short the U1 pin to the respective VDD, VSS, or GND line. For testing where control pins do not change state (such as the select or enable pin always being at a logic ‘1’ for the duration of testing), shunts can be connected on the appropriate jumpers to short the U1 control pins to VDD or GND. For the remaining I/O pins (VDD, VSS, and GND), signals can be applied using shunts in the same manner as before or the shunt can be removed and an external signal can be applied to the U1 pin of the jumper or the respective test point.

In cases where the tests requires pull-up or pull-down resistors versus directly attaching the source to the respective U1 pin, all 8 generic pathways contain 0603 resistor pads to add these components. Table 3-2 shows the IDs.

Table 2-2 Pull-Up or Pull-Down Resistor Configuration Map
0603 Sized Resistor Pad IDJumper ID

Function

R1

J1

Pull up

R13

J1

Pull down

R2

J2

Pull up
R14

J2

Pull down
R3

J3

Pull up
R15

J3

Pull down

R4

J4

Pull up

R16

J4

Pull down

R34

J5

Pull up

R40

J5

Pull down

R33

J6

Pull up

R39

J6

Pull down

R17

J7

Pull up

R29

J7

Pull down

R18

J8

Pull up

R30

J8

Pull down

R19

J9

Pull up

R31

J9

Pull down

R20

J10

Pull up

R32

J10

Pull down

Now loads can be attached to the board. If a pull-down pad was unused, then this pad can now be used as a pad for a resistive load. There are also pads for capacitive loads for each of the 10 generic signal pathways that can also be utilized. Table 3-3 shows the corresponding pad and jumper IDs.

Note: The 1812 sized capacitor pads are on the bottom side of the EVM.
Table 2-3 RC Load Configuration Map

Jumper ID

0603 Sized Resistor Pad ID

1206 Sized Capacitor Pad ID

1812 Sized Capacitor Pad ID

J1

R13

C11

C7

J2

R14

C12

C8

J3

R15

C13

C9

J4

R16

C14

C10

J5

R40

C26

C24

J6

R39

C25

C23

J7

R29

C19

C15

J8

R30

C20

C16

J9

R31

C21

C17

J10

R32

C22

C18

Now that the loading is complete for the board, additional supply decoupling capacitance to ground can be added for the VDD or VSS lines. Table 3-4 shows the power supply decoupling capacitance for each VDD or VSS line. If the default capacitance is enough, then move on to step 8.

Table 2-4 Capacitors
Capacitor Pad IDPad Size (LxW)Associated Power Signal

C1

6mm × 5mm

VDD

C2

6mm × 5mm

VDD

C5

6mm × 5mm

VSS

C6

6mm × 5mm

VSS

Finally, attach the supply signals (VDD, GND, or VSS) to the appropriate pins of the terminal block labeled J11. Power is now ready to be applied to the board. For test points, please see the next section.