SLAAE88B December 2022 – March 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
The NON-MAIN configuration can be done with Sysconfig. Here is an example how to disable PA18 BSL invoke function in NON-MAIN flash, for PA18 is used for BSL invoke by default settings in NON-MAIN. If the application do not use the PA18 as the BSL invoke, this pin must be pull down or disable its BSL invoke function in NON-MAIN to avoid the device to into BSL mode when power up or reset.