SLAAE88B December 2022 – March 2024 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
When the ROM-based BSL interface section settings can’s meet the application’s requirement. The flash-based plug-in interface demos can be used. Due to the code for the communication section are both open source, customer can change any settings in the code. Remember that the flash-based plug-in interface demos can only receive the BSL packets and not parse the packets. So, the plug-in interface demos need to co-work with BSL core located in the ROM BSL to parsing the commands.