SLAAEK1 April 2024 AFE432A3W , AFE532A3W , DAC530A2W , DAC532A3W
Key Input Parameter | Key Output Signal | Recommended Device |
---|---|---|
SPI or I2C communication | 0mA to 300mA programmable LED current | DAC530A2W, DAC532A3W, AFE532A3W, AFE432A3W |
Objective: Bias an LED using a programmable current source.
This design uses a buffered voltage and current output smart digital-to-analog converter (DAC) such as the DAC530A2W or DAC532A3W (DAC53xAxW) to bias a light-emitting diode (LED). The current output DAC (IDAC) on the DAC53xAxW can source up to 300mA to bias high-current LEDs. The DAC53xAxW have a general-purpose input-output (GPIO) pin that can be used to switch the LEDs between two current values, or on and off. The voltage channel of the DAC53xAxW can be configured as a comparator to monitor the LED voltage (VLED) for software-independent fault management. The output of the comparator can be connected to the DAC53xAxW GPIO pin to turn the IDAC off if VLED is out of range. All register settings can be saved into the non-volatile memory (NVM) on the smart DAC, meaning that the device can be used without a processor, even after a power cycle. This circuit can be used in applications such as in-vitro diagnostics, endoscopes, and digital microscopes.
The DAC530A2W IDAC channel can be configured for a 300mA or 220mA output range in the IOUT-GAIN field of the DAC-2-GAIN-CONFIG register. This application uses the 300mA range.
This schematic is used for the following design results of the DAC530A2W. VLED and ILED are measured at the test points marked on the schematic.
The following table shows an example register map for this application. The values given here are for the design choices made in the Design Notes section.
Register Address | Register Name | Setting | Description |
---|---|---|---|
0x03 | DAC-2-GAIN-CONFIG | 0x0000 | [15:13] 0b000: Don't care |
[12:10] 0b000: Selects 2/3 gain | |||
[9:0] 0x00: Don't care | |||
0x15 | DAC-1-GAIN-CMP-CONFIG | 0x040D | [15:13] 0b0: Don't care |
[12:10] 0b001: Set REF-GAIN-1 to 1 × VDD | |||
[9:5] 0b0: Don't care | |||
[4] 0b0: Set comparator output pin as push-pull | |||
[3] 0b1: Enable comparator output | |||
[2] 0x1: Set comparator input pin to finite impedance | |||
[1] 0x0: Do not invert the comparator output | |||
[0] 0x1: Enable comparator mode | |||
0x19 | DAC-2-DATA | 0x5740 | [15:6] 0x2DD: 10-bit IDAC code |
[5:0] 0x0: Don't care | |||
0x1C | DAC-1-DATA | 0x4D80 | [15:6] 0x136: 10-bit comparator threshold |
[5:0] 0x0: Don't care | |||
0x1F | COMMON-CONFIG | 0x13F9 | [15] 0b0: Write 0b0 to set the window-comparator output to a non-latching output |
[14] 0b0: Device not locked | |||
[13] 0b0: Fault-dump read enable at address 0x00 | |||
[12] 0b1: Enables the internal reference | |||
[11:10] 0b00: Powers up VOUT1 | |||
[9] 0b1: Reserved. Always write 1 | |||
[8:7] 0b11: Reserved. Always write 0b11 | |||
[6:3] 0xF: Reserved. Always write 0xF | |||
[2:1] 0b00: Powers up IDAC2 | |||
[0] 0b1: Reserved. Always write 1 | |||
0x20 | COMMON-TRIGGER | 0x0002 | [15:12] 0b0000: Write 0b0101 to unlock the device |
[11:8] 0b0000: Write 0b1010 to trigger a POR reset | |||
[7] 0b0: LDAC is not triggered | |||
[6] 0b0: DAC clear is not triggered | |||
[5] 0b0: Don't care | |||
[4] 0b0: Fault-dump is not triggered | |||
[3] 0b0: PROTECT function not triggered | |||
[2] 0b0: Fault-dump read not triggered | |||
[1] 0b1: Write 0b1 to store applicable register settings to the NVM | |||
[0] 0b0: NVM reload not triggered. Write 0b1 to reload applicable registers with existing NVM settings | |||
0x24 | GPIO-CONFIG | 0x002F | [15] 0b0: Glitch filter disabled for GP input |
[14] 0b0: Don't care | |||
[13] 0b0: Disable output mode for GPIO pin | |||
[12:9] 0b0000: Selects the STATUS function setting mapped to GPIO as output | |||
[8:5] 0b0001: Enables GPI function on channel 2 | |||
[4:1] 0b0111: GP input configured to trigger clear | |||
[0] 0b1: Enables input mode for GPIO pin |
The following shows a pseudocode sequence to program the initial register values to the NVM of the DAC530A2W. The values given here are for the design choices made in the Design Notes section.
Pseudocode Example for DAC530A2W
//SYNTAX: WRITE <REGISTER NAME (Hex Code)>, <MSB DATA>, <LSB DATA>
//Set IDAC gain setting to 2/3
WRITE DAC-2-GAIN-CONFIG(0x03), 0x00, 0x00
//Write DAC code for nominal IDAC output
//The 10-bit hex code for 250mA is 0x2DD. With 16-bit left alignment, this becomes 0xB740
WRITE DAC-2-DATA(0x19), 0x57, 0x40
//Set VOUT1 gain setting to 1× VDD (3.3V), enable comparator mode, enable comparator output, disable Hi-z input
WRITE DAC-1-GAIN-CMP-CONFIG(0x15), 0x04, 0x0D
//For a 3.3V output range, the 10bit hex code for 1V is 0x136. With 16-bit left alignment, this becomes 0x4D80
WRITE DAC-1-DATA(0x1C), 0x4D, 0x80
//Power-up output on IDAC and VDAC channels, enables internal reference
WRITE COMMON-CONFIG(0x1F), 0x13, 0xF9
//Configure GPI for clear trigger for IDAC channel
WRITE GPIO-CONFIG(0x24), 0x00, 0x2F
//Save settings to NVM
WRITE COMMON-TRIGGER(0x20), 0x00, 0x02
Device | Key Features | Link |
---|---|---|
DAC530A2W | 10-bit 300mA current-source DAC with supervisor comparator or VDAC channel, NVM and GPIO | DAC530A2W |
DAC532A3W | 10-bit 300mA current-source DAC with 10-bit voltage-output DAC, supervisor comparator, NVM and GPI | DAC532A3W |
AFE532A3W | 10-bit 300mA current-source DAC with 10-bit SAR ADC, 10-bit VDAC, NVM and GPI | AFE532A3W |
AFE432A3W | 8-bit 300mA current-source DAC with 10-bit SAR ADC, VDAC, NVM, and GPI | AFE432A3W |
Find other possible devices using the parametric search tool.
See Analog Engineer's Circuit Cookbooks for TI's comprehensive circuit library.
Additional Resources
For direct support from TI Engineers, use the E2E™ forums: