SLUAAK3 January   2024 UCC256402

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2UCC25640X HS Pin Has Wide dv/dt Sensing Range
  6. 3UCC256402/4 Eliminating the Need for the Auxpower
  7. 4UCC25640X has Higher Vcc Startup Voltage to Support Lower Vcc Capacitance
  8. 5UCC25640X has Programmable Burst Mode Threshold
  9. 6UCC256402A Supports Input OVP to Protect PSU if Grid Voltage is Unstable
  10. 7UCC25640X has Diversity Version for Each Application
  11. 8Summary
  12. 9References

Trademarks

All trademarks are the property of their respective owners.