SLVUCP9A November   2023  – March 2024 TPS25751

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Power Requirements
    2. 2.2 Setup
    3. 2.3 Header Information
    4. 2.4 Jumper Information
    5. 2.5 LED Information
    6. 2.6 Test Points
    7. 2.7 Switches/Push Buttons
  9. 3Software
    1. 3.1 Software Description
      1. 3.1.1 Software Installation
      2. 3.1.2 Web Browser
      3. 3.1.3 Native Application
    2. 3.2 Software Development
    3. 3.3 Using the TPS25751 Application Customization Tool
      1. 3.3.1 Default View
      2. 3.3.2 Selecting a Configuration
      3. 3.3.3 Filling Out the Questionnaire
      4. 3.3.4 Advanced Configuration Mode
      5. 3.3.5 Flashing Configuration onto EVM
      6. 3.3.6 Additional Settings
        1. 3.3.6.1 Generating a New Configuration
        2. 3.3.6.2 Exporting and Importing Settings
        3. 3.3.6.3 Generating the Binary
        4. 3.3.6.4 Generating the VIF file
  10. 4Application Specific Use Case
    1. 4.1 Application Specific General Overview
    2. 4.2 TPS25751EVM and BQ257xxEVM Setup
      1. 4.2.1 Setting up with BQ25756(E)EVM
        1. 4.2.1.1 Hardware Setup with BQ25756(E)EVM
        2. 4.2.1.2 Software Setup with BQ25756(E)EVM
      2. 4.2.2 Setting up with BQ25792/8EVM
        1. 4.2.2.1 Hardware Setup with BQ25792/8EVM
        2. 4.2.2.2 Software Setup with BQ25792/8EVM
      3. 4.2.3 Setting up with BQ25713EVM
        1. 4.2.3.1 Hardware Setup with BQ25713EVM
        2. 4.2.3.2 Software Setup with BQ25713EVM
    3. 4.3 Liquid Detection and Corrosion Mitigation Overview
      1. 4.3.1 Liquid Detection/Corrosion Mitigation Hardware Setup
      2. 4.3.2 Liquid Detection/Corrosion Mitigation Software Setup
  11. 5Hardware Design Files
    1. 5.1 Schematics
    2. 5.2 PCB Layouts
    3. 5.3 Bill of Materials (BOM)
  12. 6Additional Information
    1. 6.1 Trademarks
    2. 6.2 Electrostatic Discharge Caution
    3. 6.3 Terminology
    4. 6.4 Device Support
      1. 6.4.1 Third-Party Products Disclaimer
      2. 6.4.2 Supplemental Content
    5. 6.5 Documentation Support
      1. 6.5.1 Documentation Support
    6. 6.6 Receiving Notification of Documentation Updates
    7. 6.7 Support Resources
  13. 7Revision History

Filling Out the Questionnaire

After selecting the TPS25751 configuration, continue to fill out the remaining questions to flash or generate a full configuration. Based on the selection for Question 1, some of the remaining questions can be unavailable for selection.

Questions 2 through 4 asks for the maximum power that is sourced or sinked. If a source-only configuration was selected in Question 1, then Question 3 is not available to select. If a sink-only configuration was selected, then Question 2 is not available to select. Question 4 determines the power role preference of TPS25751, this question is only available if the system is DRP (Dual Role Power).

When selecting the maximum power that can be sourced or sink, this configures the Transmit Source Capabilities (0x32) and Transmit Sink Capabilities (0x33) register of TPS25751 by adding default Source/Sink PDOs. The voltage and current rating applies for both Source and Sink PDOs. See the figure below for the default configuration.

GUID-20231109-SS0I-D2NK-WN6Z-NMC7FBFWHDMC-low.svg

Question 5 asks for the supported USB speed. Based on the selection, this determines what USB speed is enumerated during PD negotiation. If USB data is not required, then select No USB data is being used.

Question 6 asks for the preferred data role. Based on the selection, this determines the data role (UFP, DFP, or DRP) TPS25751 is configured for. If there is no preference, then select No.

Question 7 asks for BC1.2 and legacy charging support. Based on the selection, TPS25751 can enumerate different BC1.2 charging schemes. Refer to the TPS25751 data sheet for more details.

Question 8 asks for Liquid Detection support. This is a new feature of TPS25751 based on the Type-C specifications for Liquid Detection and Corrosion Mitigation. Refer to Section 4.3 for more details.

Note: TPS25751 is not able to support BC1.2 and Liquid Detection simultaneously since both features utilize the same GPIO pins.

Questions 9 and 10 asks for the Vendor ID and the desired Product ID respectively. The Vendor ID is given by the USB-IF and the Product ID is simply a configuration identifier. Select Yes option to enter 4-digit hexadecimal number, otherwise select No.

GUID-20231109-SS0I-HLDW-GL1F-7FTBFKXSD3XT-low.svg

Questions 11 through 18 corresponds to configuring the selected BQ (Battery Charger) device if applicable. These questions are only available for filling in if a BQ configuration was selected in the first question. For all other non-BQ configuration (TPS25751 only), these questions are disabled. Refer to Section 4.2 section for more details on each questionnaire and the applications.