SNVA213B May 2007 – February 2022 LM2745
When the tracking feature of the LM2745 is required for use, remove the jumper that connects the soft-start capacitor, C10, and connect the resistor divider, on designators R13 and R14 (see Figure 3-1). The Track terminal has been provided for the user's connecting convenience. The demo board is synchronize ready, just connect an external clock to the SYNC terminal.
Monitor the MOSFET junction temperature since switching losses will increase, and do not exceed the maximum junction temperature of the MOSFET. Refer to the MOSFET manufacturer data sheet for the maximum junction temperature specification and heat sinking guidelines.