SPRACX0 March 2021 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P550SJ , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
//----------------------------------------------------------------------
// CMPSS5H Capture ZVS (Inductor current NZC)
//----------------------------------------------------------------------
//setup analog input of CMPSS 5, connect inductor current signal to CMPSS5
ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_5, 2);
// Power up Comparator locally
CMPSS_enableModule(base5);
// Connect the inverting input to internal DAC. Invert CMPH output.
CMPSS_configHighComparator(base5, CMPSS_INSRC_DAC|CMPSS_INV_INVERTED);
// Set DAC output
CMPSS_setDACValueHigh(base5, (int16_t)(iL_limit));
// DACHVALA is updated from DACHVALS (no Internal ramp)
CMPSS_configDAC(base5, CMPSS_DACSRC_SHDW);
// Output = asynch comparator output (output inverted)
CMPSS_configOutputsHigh(base5, CMPSS_TRIP_ASYNC_COMP);
// Xbar setting
//------------------------------------------------------------------------
// CMPSS5H – ZVS (Inductor current NZC)
//------------------------------------------------------------------------
XBAR_setEPWMMuxConfig(XBAR_TRIP5, ZVS_CAPTURE_XBAR_MUX_CONFIG);
XBAR_enableEPWMMux(XBAR_TRIP5, ZVS_CAPTURE_XBAR_MUX);
//Clear XBAR flag during initialization
XBAR_clearInputFlag(XBAR_INPUT_FLG_CMPSS2_CTRIPH);
//***********************************************************************************
// Configure PWM1A for switching Frequency and valley switching.
//***********************************************************************************
// ZVS(Inductor current NZC) related registers setup starts here
// Select one of the DCAEVT1 events as input to the event filtering logic block
EPWM_setDigitalCompareFilterInput(base1, EPWM_DC_WINDOW_SOURCE_DCAEVT1);
// Edge filter is selected
EPWM_enableDigitalCompareEdgeFilter(base1);
// Edge mode is selected
EPWM_setDigitalCompareEdgeFilterMode(base1, EPWM_DC_EDGEFILT_MODE_BOTH);
// Edge count is selected
EPWM_setDigitalCompareEdgeFilterEdgeCount(base1,1);
//Software trigger (triggered in ISR)
EPWM_setValleyTriggerSource(base1, EPWM_VALLEY_TRIGGER_EVENT_SOFTWARE);
//valley capture enabled
EPWM_enableValleyCapture(base1);
//DELAY applied
EPWM_enableValleyHWDelay(base1);
//SW DELAY duration
EPWM_setValleySWDelayValue(base1, SWDELAY);
// DCAH = Comparator 5 output = TRIP5in
EPWM_selectDigitalCompareTripInput(base1, EPWM_DC_TRIP_TRIPIN5,EPWM_DC_TYPE_DCAH);
//DCAH = high (1 TBCLK wide pulse is generated by edge filter)
EPWM_setTripZoneDigitalCompareEventCondition(base1, EPWM_TZ_DC_OUTPUT_A1,
EPWM_TZ_EVENT_DCXH_HIGH);
//Source is filtered DCAEVT1
EPWM_setDigitalCompareEventSource(base1, EPWM_DC_MODULE_A, EPWM_DC_EVENT_1,
EPWM_DC_EVENT_SOURCE_FILT_SIGNAL);
//Async
EPWM_setDigitalCompareEventSyncMode(base1, EPWM_DC_MODULE_A, EPWM_DC_EVENT_1,
EPWM_DC_EVENT_INPUT_NOT_SYNCED);
//Use blanking window to filtering PZC edge and noise
EPWM_enableDigitalCompareBlankingWindow(base1);
EPWM_setDigitalCompareBlankingEvent(base1, EPWM_DC_WINDOW_START_TBCTR_ZERO);
// Blanking Window Offset = CMPA(n+1)
EPWM_setDigitalCompareWindowOffset(base1, 1);
// Blanking window length
EPWM_setDigitalCompareWindowLength(base1, MIN_PERIOD);
// Enable time-base counter capture
EPWM_enableDigitalCompareCounterCapture(base1);
//ZVS code stops here