SPRACY9 March   2023 TMS320F2800132 , TMS320F2800132 , TMS320F2800133 , TMS320F2800133 , TMS320F2800135 , TMS320F2800135 , TMS320F2800137 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280023C , TMS320F280025 , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280033 , TMS320F280034 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C , TMS320F280049C-Q1 , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28076 , TMS320F28374D , TMS320F28374D , TMS320F28374S , TMS320F28374S , TMS320F28375D , TMS320F28375D , TMS320F28375S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376D , TMS320F28376S , TMS320F28376S , TMS320F28377D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378D , TMS320F28378S , TMS320F28378S , TMS320F28379D , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28379S , TMS320F28384D , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388D , TMS320F28388S , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1 , TMS320F28P659SH-Q1

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
    1. 1.1 Mechanism of ADC Input Settling
    2. 1.2 Symptoms of Inadequate Settling
      1. 1.2.1 Distortion
      2. 1.2.2 Memory Cross-Talk
      3. 1.2.3 Accuracy
      4. 1.2.4 C2000 ADC Architecture
    3. 1.3 Resources
      1. 1.3.1 TINA-TI SPICE-Based Analog Simulation Program
      2. 1.3.2 PSPICE for TI Design and Simulation Tool
      3. 1.3.3 TI Precision Labs - SAR ADC Input Driver Design Series
      4. 1.3.4 Analog Engineer's Calculator
      5. 1.3.5 Related Application Reports
      6. 1.3.6 PSpice for TI ADC Input Models
  4. 2Input Settling Design Steps
    1. 2.1 Select the ADC
    2. 2.2 Find the Minimum Op-Amp Bandwidth and RC Filter Ranges
      1. 2.2.1 Select Type
      2. 2.2.2 Resolution
      3. 2.2.3 Csh
      4. 2.2.4 Full-Scale Range
      5. 2.2.5 Acquisition Time
      6. 2.2.6 Outputs
      7. 2.2.7 Math Behind the Calculator
    3. 2.3 Select an Op-Amp
    4. 2.4 Verify the Op-Amp Model
    5. 2.5 Build the ADC Input Model
      1. 2.5.1 Vin
      2. 2.5.2 Voa, Voa_SS, and Verror
      3. 2.5.3 Rs, Cs, and Vcont
      4. 2.5.4 Ch, Ron, and Cp
      5. 2.5.5 S+H Switch, Discharge Switch, tacq, and tdis
    6. 2.6 Refine RC Filter Values Via Simulation
    7. 2.7 Perform Final Simulations
    8. 2.8 Input Design Worksheet
  5. 3Example Circuit Design
    1. 3.1  Select the ADC
    2. 3.2  Find the Minimum Op-Amp Bandwidth and RC Filter Ranges
    3. 3.3  Verify the Op-Amp Model
    4. 3.4  Build the ADC Input Model
    5. 3.5  Bias Point Analysis to Determine Voa_ss
    6. 3.6  Transient Analysis to Determine Voa_ss
    7. 3.7  Perform Initial Transient Analysis
    8. 3.8  Iterative Approach to Refine RC Filter Values
    9. 3.9  Perform Final Transient Analysis
    10. 3.10 Perform Final Transient Analysis
    11. 3.11 Further Refinement
    12. 3.12 Further Simulations
    13. 3.13 Completed Worksheet
  6. 4Working With Existing Circuits or Additional Constraints
    1. 4.1 Existing Circuits
      1. 4.1.1 Brief Overview of Charge Sharing
      2. 4.1.2 Charge Sharing Example
      3. 4.1.3 Additional Resources for Charge Sharing
    2. 4.2 Pre-Selected Op-Amp
      1. 4.2.1 Pre-Selected Op-Amp Example
    3. 4.3 Pre-Selected Rs and Cs Values
      1. 4.3.1 Analytical Solution for ADC Acquisition Time
      2. 4.3.2 Example Analytical Solution for ADC Acquisition Time
  7. 5Summary
  8. 6References

Iterative Approach to Refine RC Filter Values

Now that the basic simulation has shown that the simulation is fundamentally working, sweeps can be performed to refine the Rs component selection.

To perform a sweep, open the transient simulation profile and enable the Parametric Sweep option. In the Parametric Sweep settings, choose the global parameter R_STEP as the sweep variable. Then choose a linear sweep type with a start value of 17 Ω, an end value of 138 Ω, and an increment of 10 Ω as shown in Figure 3-12.

GUID-513E3FE0-D177-475C-BE17-8B5AE9E7E2D0-low.jpg Figure 3-12 F280049 Example Parametric Sweep Settings

After performing the analysis, delete all outputs other than Verror and set Verror range to -30 mV to +30 mV. Additionally, limit the waveform to +2.95 µs to +3.15 µs to better observe the settling. Alternatively, go to Window ➔ Display Control... using the menu in the upper left of the PSpice for TI simulation window to access a list of preset display configurations provided by TI. Restore the Sweep Results display configuration. Note that these preset display configurations are only available in the PSpice for TI projects bundled with this application report. Figure 3-13 shows the output of the transient simulation with a sweep of Rs.

From this output, it can be concluded:

  • Higher resistance values in the Rs range do not provide quick enough settling. For instance, 107 Ω only settles to 6.1 mV in the allocated S+H time while the settling target is 366 µV
  • A good range for further investigation would be 20 Ω to 60 Ω. Determining the optimal value of Rs requires further analysis, which may include additional simulations

GUID-CE8C423F-FFB5-47B8-A02E-FFD15DC5B726-low.jpg Figure 3-13 F280049 Example Rs Initial Sweep Results

Based on the initial sweep results, it may already be possible to identify one or more values of Rs that provide adequate settling. If desired, the Rs component selection can be further refined by iteratively narrowing the linear sweep range. A value list sweep may also be performed to test values of Rs that are not linearly spaced. An example simulation profile for a value list sweep is shown in Figure 3-14.

GUID-A4D5194E-EC8E-4D2C-9403-E4C812C0EF8C-low.jpg Figure 3-14 F280049 Example Parametric Sweep Settings

Thus, a final value of Rs can be selected that provides adequate settling. With enough iterations, the final value of Rs can be made optimal. However, Section 3.9 introduces an alternative method to better select the optimal value of Rs using the Performance Analysis tool.